A-IoT
Leopard Imaging redefines visual IoT with powerful cameras and AWS cloud technology
Leopard Imaging’s latest and greatest camera technology is integrated with smart control systems to create advanced IoT-based systems. In applications like smart homes, smart lamps, vehicle asset tracking, smart traffic control systems, and visual security alarm systems, Leopard Imaging IoT-based camera solutions excel.
Thanks to our highly capable camera hardware designed specifically for IoT-based applications such as DEV-16260 ROHS, and years of system integration, we offer the best-in-class IoT systems for your custom needs. Visual IoT applications have key imaging requirements for the supporting camera hardware such as high-definition image/video, excellent low-light performance, a robust HDR processing pipeline for challenging light conditions, and a global shutter to capture fast-moving objects without artifacts or motion blur.
Leopard Imaging provides IoT solutions supported by visual technology that satisfies all key imaging requirements according to the challenge at hand. Leopard Imaging is proud to work with its official cloud partner AWS for its cloud computing applications. All Leopard Imaging IoT-based camera systems communicate seamlessly with the AWS cloud. We also offer AWS-supported hardware for fast local inference and processing, perfect for real-time health monitoring systems using IoT-based cameras.
In certain applications, the information collected by sensors needs to be processed at a fast rate but cannot be done by local hardware. For that purpose, Leopard Imaging utilizes cloud computing.
Leopard Imaging works in conjunction with its lens partners, industry-leading processor manufacturers, and world-class AI platform partners to build for you a complete IoT solution. The solution comprises an elegant integration of multiple sensors, cameras, processing power, and other technologies.
IoT cameras and the solutions built in this collaboration are high-performance and more than reliable. Home surveillance systems using IoT are becoming more commonplace than ever, for which Leopard Imaging IoT-based camera systems can be employed by domestic and commercial clients alike. Leopard Imaging works in conjunction with its lens partners, industry-leading processor manufacturers, and world-class AI platform partners to build for you a complete IoT solution. The solution comprises an elegant integration of multiple sensors, cameras, processing power, and other technologies.
IoT cameras and the solutions built in this collaboration are high-performance and more than reliable. Home surveillance systems using IoT are becoming more commonplace than ever, for which Leopard Imaging IoT-based camera systems can be employed by domestic and commercial clients alike.